Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Cable carriers for indoor cranes

This elaborate roof construction is an example of how energy chain cable carriers can be used in special designs.

Retractable pool roof

A retractable 131 ft (40 m) x 131 ft (40 m) roof for an indoor/outdoor swimming pool is operated via 25 chainflex® continuous-flex cables inside an energy chain cable carrier.

Thanks to this design, about 328 ft (100 m) of cable was saved and the overall weight of the roof was reduced. A cable carrier system also had to be used because of the limited installation space available: 3.28 ft (1 m).

The harsh environmental conditions have not posed a problem for the maintenance-free roof structure for several years.
igus® E2 type series Cable carrier for crane used in indoor/outdoor environment

Aluminum guide trough

In spite of the sophisticated technology, the cable carrier system is the most aesthetically suitable solution which also copes well with the adverse conditions.

The environmental conditions for the indoor/outdoor pool are harsh: the water is treated with an oxygen-chlorine mix which is evaporated into the air in which the cable carrier is working. To counter the threat of corrosion, an aluminum guide trough was selected for the cable carriers.

System E2 (series 250 and 350/3500) energy chain cable carriers were used.
The semi-finished crane structure, with an igus® cable carrier The semi-finished crane structure, with an igus® cable carrier from the E2/000 range

More product information

More application examples from different industries



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302