Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Linear guides for handling equipment

The demand to produce smaller and smaller products requires highly accurate handling devices that can be quickly retrofitted. These devices should also be space efficient. One such device suitable for various industrial sectors uses igus® linear guides, which are lubrication-free and so save time spent on maintenance work.

Glides instead of rolling

drylin® R linear bearings, drylin® W modular guides, drylin® T profile rail guides, and drylin® N low profile linear guides from igus® are all used in this handling device.

In contrast to recirculating linear ball bearing systems, the drylin® linear guides move on high performance plastic gliding elements made from the igus® plastic iglide® J, which is low wear and low friction.

drylin® linear bearing systems are designed for dry operation, so dirt accumulation is not an issue. In contrast with recirculating ball bearing systems, drylin® guides do not require a minimum stroke or travel length.
linear bearings This handling device is suitable for workpieces up to maximum 11 lbs and runs in cycles of less than 0.5 seconds.
profile rail guides igus® offers a comprehensive product range that also includes the simplest guide systems for pneumatic cylinders
linear guide Positioning and supply system: the nicknamed "never-ending axis"

More on the linear products used

More bearings applications from different industries

Useful Links



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302